Hi,
I was curious to know if the SSI interfaces supported by both the ADS7816 ADC and the ARM LM3S3748 microprocessor are compatible with one another. And, if so, what framing format does the ADS7816 implement: TI, Freescale or Microwire. The timing diagram in the ADS7816 data sheet seemed to be most close to Freescale where data is clocked on the falling edge, but I wasn't sure. Ultimately I am just looking for an ADC having an SSI interface compatible with the LM3S3748 that is offered in a DIP package. So, if there is a better chip than the ADS7816, I would be interested to learn about it.
Thanks!
Court