This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC60508: output voltage range - when reference divider issues a reference alarm condition and set the output to zero

Part Number: DAC60508


Tool/software:

Hi,

I want to work with voltage output of 5V with VDD of 5V.

The VDD is not promised to be over 5V and could be a bit under this value (could be 4.75V).  

what is the value the reference divider issues a reference alarm condition and set the output to zero?

I didn't have a problem to work with the range of 0V to VDD if VDD is above 4.75V.

Pls. advise

Zeev Gerber