This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC39RF10: CAN I use JMODE=2 for 1 real data stream?

Part Number: DAC39RF10


Tool/software:

To the TI Support Team,

CAN I use JMODE=2 for 1 real data stream without interpolation, LT=1?

The number of lanes to use is 4.

With the above configuration, I can not select JMODE of 2 in the DAC39RF1xEVM GUI.

the update Rate is 1.0GHz, DAC resolution is 16 bit, JSED protocol is 8b10b and subclass is 1.

Best regards,
Jeongju Go