Tool/software:
It is indicated in the datasheet SBAS691B –MARCH 2016–REVISED OCTOBER 2018 of ADS1282-SP page 40:
"After a register write operation the ADC resets, resulting in an interruption of 63 readings"
1/ What is the meaning of this interruption ? Not possible to send commands through SPI ? Not possible to acquire values ? What can we do during this interruption ?
2/ Duration of the interruption: 63 readings = 63 / Fdata =~ 16 ms for 4000 SPS ?
3/ Start of the timing is from the end of the last byte of the command ?