Tool/software:
Hi
If input signal slew rate is 5V/ns then what will be output slew rate when translating down as below with 100 MHz frequency.
Case1: 3.3V to 0.8V (A to B)
Case2: 3.3V to 2.5V (A to B)
Will it keep maintain same slew rate 5V/ns or any deviation will be there ?
Best regards