I have to convert a fast repetitive step-like signal applied as an input to the ADS58B18EVM in single-ended mode (through the already installed J6 SMA connector).
My first question is: what output impedance my signal source should have to match TI's EVM input impedance? I've looked to the schematics and BOM and I'm a bit confused about why J6 SMA connector has an impedance of 50 ohms, while ADT1-1WT input transformer has a characteristic impedance of 75 ohms, so I couldn't find out this information by myself.
Moreover, I couldn't find on the board user manual informations about the two DNI resistors R22 and R25: what is their function? In which case should I install them?
I've got also another question: how high could my input frequency be for my signal to be not distorted before coming to the ADC input pins? If I needed to DC couple my input signal on J6 connector to the ADC input pins (IN_P and IN_M on the board schematics), could I simply uninstall the two transformers T1 ad T2 or what issues should I care about? What would you suggest?
Thank you in advance for any help you will give me.
Regards,
Lorenzo