Part Number: ADC12D1620QML-SP
Other Parts Discussed in Thread: THS4541
Tool/software:
Hi,
My custoner is facing following problem.
* Customer use ADC12D1620 for their application. customer is now observing approx 800h even though they input analog data (approx 500mVpp)
Here are information for their configuration.
- Customer input 500MHz clock to ADC
- Customer confirmed 250Mhz output on DCLK pins ("SDR", "Non-DES mode" and "1:2 demux" setting)
- They could observe expected output when they use test pattern (enabling "TPM").
- Customer observe approx 800h output data both no analog input and certain analog input (500mVpp)
(In fact, custoner observed from 7f9h to 807h)
I noticed even though customer connect "Vcmo" pin to "GND" (mean "AC coupled" input), they did not input AC coupling capacitor on analog input line (Vinl, Vinq).
Also, ADC driver's common mode voltage is set as "0V".
Then I have following question.
Q1. According to datasheet, when user set "AC coupled input", it seems that 1.25V is applied as common mode voltage for analog input.
When analog input with 0V common mode voltage is applied to analog input without AC coupling, is phenomenon which we observe middle value(800h) on digital output expected behavior ?
Note : I would like customer to confirm whether when they add AC coupling on analog input line, the phenomenon will be improved. However, due to issues on customer's environment, they need to obtain evidence before checking waveform and changing circuit. Therefore, I asked above question.
Best Regards,