Other Parts Discussed in Thread: LMK1C1108
Tool/software:
Hi Team,
My board clock requirement block diagram is attached below.
The clock from the clock synthesizer need to feed as input clock to all ADC, DAC and FPGA in the board to make a synchronization.
Also from FPGA an input SYNC IN/ LDAC like input signal is fed to all the ADCs and DACs so that FPGA can control and sync activities of all the data converters.
My DAC required output range is +/-1.85V.

Can i use the DAC3484 for my application.
If yes please suggest an output buffer amplifier to DAC IC so that i need a single ended output to be connected to a SMA connector.
Please provide an update on above mentioned query.
Regards,
Abhishek