Part Number: RC4580
Hi,
We are using the TI operational amplifier RC4580IDR in our product.
As shown in the attached circuit diagram, there is a situation where the op amp’s supply pins (+V, –V) are left floating (no power applied), while an external measurement instrument (LCR meter: 1 Vrms, 1 kHz) applies voltage to the output pin (OUT).
In this condition, could the RC4580IDR be damaged or degraded due to reverse current flowing into the device through internal protection structures?
Also, should such usage be strictly avoided, and if so, do you have any recommended countermeasures (such as series resistors or external protection diodes) to ensure safe operation?
We would greatly appreciate your guidance.
Best regards,
Conor