This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3562: Regarding the E-fuse loading of the ADC3562

Part Number: ADC3562
Other Parts Discussed in Thread: ADC3664

This is a question regarding the E-fuse loading of the ADC3562. In the thread "ADC3562: Propagation delay: the sampling clock falling edge to DCLK rising edge," Luke Allen-san commented, "0x13 0x1 //Efuse reload, no need to write 0x0 when done," indicating that there is no need to write 0x00. However, Table 8-8, STEP 2 on page 48 of the datasheet states that after waiting 1ms, 0x00 should be written to 0x13. There is a discrepancy between the datasheet and this comment. Which is correct regarding the necessity of writing 0x00 to the E-fuse?