This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS6422: Output load capacitance

Part Number: ADS6422
Other Parts Discussed in Thread: SN65LVDS100

Hi! I am designing a pcb that interfaces an ADS6422 with a xilinx 7 series fpga. My question is related to external load capacitance of the adc. In the datasheet it is stated that in the case of not using internal termination on the adc, the maximum load capacitance is 5 pF. Nevertheless, i have read in xilinx docummentation that the FPGA input capacitance is 8 pF. I was wondering if i should place something (a buffer or other alternatives) between the adc and the fpga to drive the external load capacitance.