Part Number: DAC7760
Other Parts Discussed in Thread: DAC8760EVM, TIPD153
Dear Sir,
Can you please explain the following points :-
- What is loop compliance Voltage , how to measure the same.
- It has been mentioned that "AVSS TIED TO GND". Can you please elobrate which ground pin to be connected and procedure to connect the AVSS TO GND.
- In the Voltage output - Load Conditions - You has ased us to add 4nf external compenstation capacitor. Can you porvide to which pins do we have to connect
- You have mentioned DC OUTPUT IMPEDENCE AS 0.3Ohms at CODE =0X8000- CAN you elborate on this.
- What is the Iset Resistor has been menitioned by you as 15KOhm low drift resistor . Can you mention the part no. of specifciation of the Resistor.
- Where Shall we connect the VSENSE PIN TO VOUT . In our Cirucit We are having a diode to protect the Vout pin , if any voltage is applied to Vout pin. We have attached a circuit for your reference can you please suggest where to connect Vout pin

- What is the loop compliance voltage and how to mesure it.
- You have asked us to connect external compensation capacitor of 4nF. Where shall it be connected and what is the use.
- What is the maximum connectable load on Iout . RL for Iout.
- You have suggested 5Kohm to connect between Vout and Vsesne. Where as in the application circuit its 15 Ohms , which shall be used.
- We have Boost Circuit that is attached for your reference . Please confirm wether the circuit is correct or not.

- We have used MJD31CTF Transistor , please suggest if that is ok or do you recommend an alternate part.
- We are not using HART Communication , How shall we connect the Hart pin directly to ground or shall be left open.
- What shall be status of NC Pin. Shall it be left open or connected to ground.
- We are only connecting Vout and Vsense . I that scenario what shall be short circuit current limiting solution please confirm. The short circuit current limiting protection given in your application notes cannot be used as there are space constraints.