This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3444: Application Inquiry

Part Number: ADC3444

Hello Experts,

I want to test the ADC3444 converter with the following input frequencies 191 MHz, 90MHz and 70 MHz but since my sampling frequency is 120MSPS will i get the desired output and parameter values ?

Are the SINAD/SNR, NSD, SFDR, ENOB parameter valus vaild if i give input frequency more then the fs/2 range?

Regards,

Jaffer Sadiq