This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12D1000: Current Consumption

Part Number: ADC12D1000
Other Parts Discussed in Thread: TPS7A53B, TPS7N49, TPS7A53

Hello,

I have a question regarding the current consumption.
According to datasheet supply current is 2.105A for ADC12D1000.
What is the margin that I have to use for the power supply in this case?
Can I use 2.105A as the max value?

I am planing to use TPS7A53B to suppply this ADC. However, the temperature is very high, also i want to keep the current 70% of the Iout max of 3A (2.1Ain this case).
image.png 

Thank you!