This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8353-Q1: VOL mismatch

Part Number: ADS8353-Q1

Hi team,

If I use VDD=5.0V, then VOL of ADS8353-Q1 is 0.2*VDD=1.0V 

while the MCU VIL=0.8V. 

Do I need a level shifter to communicate with this device?

 

If VDD=3.3V, I need a level shifter since MCU is 5V I/O device. 

 

regards,