Part Number: ADC12DJ5200RFEVM
Other Parts Discussed in Thread: TSW14J58EVM, LMX2594
Dear Technical Support Team,
I changed onboard clock from external clock (default).
We changed the clock source and connected the system to the capture board TSW14J58EVM.
However, when we clicked the Capture button, the following error occurred and the system did not operate.
Could you please advise on how to resolve this error? See attached file.
Configure ADC
SH_MB_LOCK_ERROR
Unable to obtain SH and MB lock. Please check if the ADC is configured.
The changes made compared to the configuration before changing the clock source are listed below.
Is there anything missing or incorrect?
・Circuit modifications
Removed C2, C3, C60, and C61
Installed R171 (0 Ω) and R174 (0 Ω) → shorted
Installed C52 (0.1 µF) and C306 (0.1 µF)
Removed J13
・ADC GUI settings
EVM tab
#1 Clock Source: On-board
#2 On-board Fs Selection: Fs = 5000 MSPS
Best Regards,
ttd