Part Number: AMC7908
Other Parts Discussed in Thread: AMC7904
Hi,
We are using the AMC7904 to bias a GaN PA device, with the VSS supply set to -9 V.
We observe different values in Page 1, Configuration 1 Register (offset: 0x08) depending on the DAC output load condition:
High impedance (Normal condition):
Register value = 0x01
Normal current mode (70 mA)
Low impedance / short to GND (fault condition, e.g., damaged PA):
Register value = 0x19
Indicates High current mode (130 mA) and Wide VSS configuration
Observed Issue:
When a short occurs at the DAC output, the AMC7904 automatically switches to high-current mode, increasing the current drawn from the VSS regulator.
Our goal is to limit the output current during a short condition to reduce stress on the VSS supply and improve system robustness.
Regards,
Mufeed