Hi
This is a repeated question!
workong on the AFE7225EVM evaluation card.
I want understand from what source the DAC_CLK is derived when no clock is connected to pins 8 & 9 (CLKINP/N) of the AFE7225 while there is a clock in the LVDS CLOCK INPUT : DAC_DCLKINP/N (pins: 33 & 34) as well as Frame clock : " DAC_FCLKINP/N" ( at pins : 30 $ 31)
The conditions are as in I quoted:
Digital data stream of serial 12 bits with DAC_FCLKINP @ 20 MHz and DAC_DCLKINP @ 120 MHZ
- Bitwise, 2-wires, and SDR mode.
- No clock at main clock inputs: pins 8 & 9 (CLKINP/N):, Is it Legal?
Thanks EZER