Hi,
I'm working to setup a test bench with some EVMs 6418EVM, which should be compatible with 5-6k interface board.
I need help for some informations about ADC/DAC EVM compatibility because sometimes is it not quite clear.
I have a couple basic questions:
- On a single 5-6K interface board (connected to 418 EVM) can I install 2 analog EVMs for serial interface like 1 x ADS8331EVM + 1 x DAC8331EVM (connected to McBSP 0 and McBSP 1 of the DSP) or I have limitations?
- Are ADS8361EVM and ADS8331EVM compatible with 5-6k interface board? Their connector seems to be the same apart from power supply, but this is not stated clearly. Or are they partially compatible?
Thanks for your help.