My name is Ivan and I am a researcher that works in a Neurosciences Lab with biological signals.
I write directly to you because I haven´t been able to post anything on the TI forum and I have been three days now and I am unable to do it. I have tried many times to do it from different places and browsers and when I click on post it gets stuck and stays there forever. Although I know this is not the normal procedure I hope you can help me with some problems I have regarding TI ADC/DAC converters and equipment since I am a complete novice in DSP.
We have an undergoing project for which we need a system that is able to receive a signal, process it and output in Real Time. We work with a range of frequencies that go from DC to 1000 Hz. So basically the flow would be ADC - DSP - DAC. We decided to build a modular system with a TI DSP. We bought a DSK TMS320C6416 for the processing. It already has an audio code but it filters the low frequency signals so we bought a 5-6K interface card and a ADS1174EVM and DAC8554EVM modules that are able to perform ADS-DAC conversion of low frequency signals.
Up to here, the system should be able to input a signal through the ADS1174EVM, process it in with the C6416 and output with the DAC8554EVM all in Real Time, isn´t it?.
The problem is that I am finding big problems and I am not able to make the whole system work:
1- I do know know how to connect the modules and pins in order to make it work. What about the external power that to feed the ADCs and DAC. Is there any documentation where I can take as a reference?. Could you orientate me?
2- Once everything is connected, I haven´t found any docs that make reference to the C6416 and these converters. Only some interfacing of some other ADCs and the C6713. I would like to be able to take some samples with the ADC and to output them with the DAC, just this simple operation but it seems impossible to me now. Is there any code regarding this?. I don´t, how could I do it? Maybe most of the code from the C6713 examples can be used changed for the C6416?. Are there any examples od DAC conversion with a similar system as the one I have?.
We are opened also to receive advice about other systems that could be more suitable for our purpose and more easy to work with them. Is there any other or more suitable device of TI that could do alone what we need?.
I hope you can help me with this matter since I am completely lost at this point.
Thanks in advance.
Iván