Hi,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Hi Alberto,
You are correct - the ADS8361 cannot provide data faster than 125KSPS using the single serial output mode. The ADS8363EVM is compatible with the 5-6K Interface Board. Before going to the ADS8363, can I ask if you are updating the DAC8331 at the same data rate as the ADS8361? If so, you could potentially work in Mode III using the receive side of the McBSP used on the DAC8331. Basically what you would do is set the port to use an external clock and receive an external FS. Take the CLKx from the port talking to the ADS8361 and wrap it back to CLKr on the DAC8331 side. I did something similar to this myself a few years ago during a training session we had with our field apps engineers. Take a look at the attached document for a better idea of how this might work for your project and let me know what you think.
Thanks Tom,
Hi Alberto,
Happy to hear that! The ADS8363 starts out in Mode I the same way as the ADS8361 does, so the 'synchronization' trick I showed you should work here as well. The R[1:0] bit combinations of 00 or 11 both do the same thing, internally, these bits feed an XNOR gate.