The 54AC240 part on DSCC SMD (Standard Microcircuit Drawing) 5962-87550 is shown as +/-50mA per output pin, but "DC Vcc or GND current (per pin) (ICC,IGND) is also shown as just the same +/-50mA.
Can all 8 output pins can run 50mA each at the same time, or only 50mA total across the 8?
Also, on the power dissipation limits, can you explicitly confirm that the DC power and ground pins on the device type 01 (20 pin packages) can handle 400mA for 8 output pin simulataneously driving at 50mA each total?
Thank You