Other Parts Discussed in Thread: ADS8201
When the input voltage is crossing the 2,5V with a sine wave signal, see the picture below. If the sine wave is all the time below or above the 2,5V, there is no spikes visible. Is the problem in the communication?
5V, 5V with a sine wave signal, ADS8201 iRGE. Most significant bit erroneus, see the picture below. If the sine wave is all the time below or above the 2, there is no spikes visible. Is the problem in the communication or configuration with the converter? Antti Martikainen, when the input voltage is crossing the 2