Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC3578

Other Parts Discussed in Thread: TLC3578, REF5040

Hi,

I am currently designing a circuit using TLC3578 where I have bipolar inputs of range +5V to -5V

In TLC3578 there is REFP REFM which are to connected as per datasheet via 3 capacitors

In the datasheet of TLC3578 it also states to give VREF of 4V (3.96-4.04 range)

Also in the TLC3578EVM family user guide (slau110.pdf) it is mentioned (table2-2) to give 3.3V as reference voltage

This anomaly I have not understood, as to which reference voltage to connect?

Also there is LM4030C-4.096 which can be used for 4.096V reference voltage can this be directly connected or is there any other part I am suppose to use? (i.e. is the VREF strictly required to be in 3.96-4.04 range)

Please can someone clarify the following issues?

 

Thanks Regards

Raquib Akolawala