hello:
I'am using the ADS1158, on my board ,there are 3 ADS1158 for 48th channel; I have read the datasheet, in the fixed channel mode , how to confiugurat the MUXSCH
register for channel select .for example: I want to select the second channel, the value of MUXSCH is 0x01, if i want third channel , its value is 0x30 , it's a right?
In addition, in the fixed channel mode , I read the value of s.tatus byte from the channel data format , the value is 0x9F , the BITS CHID[4:0] is the value: 1F, but it is the channel ID. why?
best regards.
edison