Hello All,
I am looking for an ADC with the below features:
Bipolar input (+/-10V range)
12-bit resolution
100 KHz sampling rate
10 microsec throughput speed
and most importantly it should operate on a single 3.3V
In the existing design, the ADC used is ADS7808 which operates on single 5V supply. But in my new design, I want to use the 3.3V technology only. I also have +/-15V supplies on the board.
I am not able to find the ADC's which can operate on 3.3V and support bipolar input range of +/-10V with any manufacturers.
Please help me in finding the suitable ADC for my new design.
Many Thanks in advance,
Kiran