ADS5402 is dual channel 800M ADC,does per ADC is single 800MADC or it is two ADCs to get interleave output? does there is the differential time delay of A,B output ?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ADS5402 is dual channel 800M ADC,does per ADC is single 800MADC or it is two ADCs to get interleave output? does there is the differential time delay of A,B output ?
thanks
It is dual 400MSPS, 800MSPS is achieved in interleave mode
Actually, ADS5402 is two channels of 800Msps each. From the front page of the datasheet:
Internal to the ADC each channel has two ADCs at 400MHz that is interleaved to provide 800Msps as shown in Figure 1 of the datasheet, so what Albert_83 said would apply to *each* channel of the device.
I do not understand what you are asking when you say "does there is the differential time delay of A,B output ?" Please clarify. If you are askign if there is skew between channel A and channel B outputs, no - they are both synchronous to the output clock and both channels will have the same latency through the ADC. From the datasheet: "Optionally Bus B can be latched with DACLKP/N." So there is an output clock for channel A and also an output clock for channel B, but these are two copies of the same clock.
Regards,
Richard P.