I have the afe5851 and to connect with the SP605 spartan6 board I buy the texas adapter card (http://www.ti.com/tool/fmc-adc-adapter). The problem is that the samtec connector of the afe5851 has 80 pins, instead the samtec in the adapter card has 120 pins, so I can't connect then. How I can do to connect the two board?
Thank you