This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Issues with using TVP5146M2

Other Parts Discussed in Thread: TVP5146M2

Hello,

I'm using TI ADC TVP5146M2 and I discover some issues:

1- Some vertical bar color appear behind the videos with a frequency around 2.3 Mhz.

the picture of this issue:

2- In RGB mode, the original colors are not restitutes correctly and depend on the video source. For example a DVD player can be use correctly in CVBS mode but don't have good color in RGB. Déactivate the AGC in AFE control register solve the problem in RGB. Is it the good process to do this or modify another register can be a better idea?

For information, registers configuration are :

- ADC

x"00" & x"CD", -- REG00 SCART - Modification 04092012

x"01" & x"0F", -- REG01 Gain Register

x"02" & x"00", -- REG02 Auto Switch Mode

x"03" & x"00", -- REG03 Normal Operation Mode

x"04" & x"3F", -- REG04 AutoSwitch to Every Possible Format

x"05" & x"10", -- REG05 Color Killer

x"06" & x"00", -- REG06 Luminance Processing 1

x"07" & x"00", -- REG07 Luminance Processing 2

x"08" & x"02", -- REG08 Luminance Processing 3

x"09" & x"A0", -- REG09 Luminance Brightness

x"0A" & x"85", -- REG0A Luminance Contrast

x"0B" & x"95", -- REG0B Chrominance Saturation

x"0C" & x"00", -- REG0C Chroma Hue

x"0D" & x"00", -- REG0D Chrominance Processing Control 1

x"0E" & x"0C", -- REG0E Chrominance Processing Control 2

x"10" & x"80", -- REG10 Component Pr Saturation

x"11" & x"80", -- REG11 Component Y Contrast

x"12" & x"80", -- REG12 Component Pb Saturation

x"14" & x"80", -- REG14 Component Y Brightness

-- PAL

x"16" & x"5F", -- REG16 AVID Start Pixel

x"17" & x"10", -- REG17 AVID Start Pixel

x"18" & x"2F", -- REG18 AVID Stop Pixel

x"19" & x"03", -- REG19 AVID Stop Pixel

x"1A" & x"00", -- REG1A HSYNC Start Pixel

x"1B" & x"00", -- REG1B HSYNC Start Pixel

x"1C" & x"40", -- REG1C HSYNC Stop Pixel

x"1D" & x"00", -- REG1D HSYNC Stop Pixel

x"1E" & x"01", -- REG1E VSYNC Start Line

x"1F" & x"00", -- REG1F VSYNC Start Line

x"20" & x"04", -- REG20 VSYNC Stop Line

x"21" & x"00", -- REG21 VSYNC Stop Line

x"22" & x"6F", -- REG22 VBLK Start Line

x"23" & x"02", -- REG23 VBLK Start Line

x"24" & x"17", -- REG24 VBLK Stop Line

x"25" & x"00", -- REG25 VBLK Stop Line

--

x"26" & x"00", -- REG26 Embedded Sync Offset Control 1

x"27" & x"00", -- REG27 Embedded Sync Offset Control 2

x"28" & x"CC", -- REG28 Fast-Switch Control Register

x"2A" & x"00", -- REG2A Fast-Switch SCART Delay Register

x"2C" & x"00", -- REG2C SCART Delay Register

x"2D" & x"00", -- REG2D CTI Delay Register

x"2E" & x"00", -- REG2E CTI Control Register

x"2F" & x"00", -- REG2F Brightness and Contrast Range Extender Register

x"32" & x"00", -- REG32 Sync Control Register

x"33" & x"00", -- REG33 Output Formatter Control 1 Register

x"34" & x"11", -- REG34 Output Formatter Control 2 Register

x"35" & x"EA", -- REG35 Output Formatter Control 3 Register

x"36" & x"AF", -- REG36 Output Formatter Control 4 Register

x"37" & x"FF", -- REG37 Output Formatter Control 5 Register

x"38" & x"FF", -- REG38 Output Formatter Control 6 Register

x"75" & x"1A" -- REG75 F-Bit and V-Bit Control 2 Register

and schematic picture of this part is: