Using the ads1241 on a number of boards with a number of different power configurations. On one of these boards the ads1241 sometimes comes up in a mode where it is does not digitize the signal correctly and results in digital codes that are too low. If you power cycle the board then the part usually works correctly. Looked at a number of power up issues including the power supply ramp and ~reset and these all look OK to me. The data sheet is not really clear as to what the different resets actually do. There are three ways to reset the chip.
1. assert the reset pin for at least the number of oscillator cycles specified on the data sheet
2. Use the special SCLK signalling sequence
3. write the RESET command (0xFE) to the SPI interface
The data sheet also says the special SCLK signaling sequence resets the entire chip but is not really clear as to what that includes.
Can someone provide some clarity about the different resets.
Regards,
John