ADS131E08 was due to be used from a customer, and there was a following two-point question.
1. If There is a "Bit Stream" by ADS131, it is the Best, but Can Such a Function be Added by External Etc.?
2. Although Analog Input Voltage is AVDD±0.3V, when AVDD±0.3V is Exceeded, is There How to Protect with Peripheral Part?
(For example, protection resistance connect to input.etc)
Thank you for your consideration.