I have following two doubts regarding performance of ADS4242
- In the datasheet of ADS4242 typical value of VCM is given as 0.95V. What is Max and min value of VCM for 2Vp-p input level without degradation of performance?
- As per datasheet, device can be configured to have channel A stand by and channel B active (Page no 25 of the datasheet, Table 7 for parallel configuration). What would be current consumption of the device is channel B is only active and A is stand by? Consider CMOS parallel output and no load capacitance