Hi, there,
I wonder if you could help me on the following design choices:
1) have Vref close to the lower limit 0.5v (but above 0.5v) with PGA=2;
2) have Vref at about 2.4V (AVDD=5V, AVSS=0V) with PGA=16.
I see that that the PGA tends to drift more over temperature as PGA value increases; is case 1) a better design than case 2)? better = more accurate and more stable over a range of temperatures.
However I am concerned that Vref close to the lower limit, which might have some adverse effect as well.
Would you please comment over these two choices?
Thank you,
Ron