This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NEED INFORMATION- V62/04615-01XE



Hi Can you please provide the following information for the  V62/04615-01XE  Part ?

1. Junction Temperature Max (Tj Max)

 2. Typical Power dissipation (Pd typ)

3. Maximum Power dissipation (Pd max)

4. Thermal Resistance Junction to Ambient (Theta JA

5. Thermal Resistance Junction to Board (Theta JB)

6. Thermal Resistance Junction to Case (Theta JC)

7. Weight

  • Good afternoon Jayakumara. To answer your questions:

    1. Junction Temperature Max (Tj Max)

    We 150C is maximum junction temerature for this technology.

     2. Typical Power dissipation (Pd typ)

    Per our device expert:

    Typ power dissipation.  P=CV^2F.   Using 20pf from operating char table, You can estimate typical power using customer frequency and voltage.

    3. Maximum Power dissipation (Pd max)

    N/A see thermal metrics and Tj/Ta max. Note device life can be affected if the device is operated continuously at maximum junction temperature.

    4. Thermal Resistance Junction to Ambient (Theta JA)

    86.0 C/W

    5. Thermal Resistance Junction to Board (Theta JB)

    44.7 C/W

    6. Thermal Resistance Junction to Case (Theta JC)

    50.7 C/W (Top)

    7. Weight

    146.500000 mg.