This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DL080 Single-Ended Operation



I'm trying to figure out how i need to connect this adc. I have 0-2V signal that i want to convert. if i understand from the datasheet:

However, if single ended-operation is required and the resulting performance
degradation is acceptable, one of the analog inputs should be connected to the d.c. mid point voltage of the
driven input. The peak-to-peak input signal at the driven input pin should be twice the reference voltage to
maximize SNR and SINAD performance (Figure 41b). For example, set VREF to 1.0V, bias VIN− to 1.5V and drive
VIN+ with a signal range of 0.5V to 2.5V.

So in my case i would need to connect Vin- to 1V and drive the Vin+ withy my 0-2V signal. Is this correct? 

  • Yes, you are correct that Vin- should be 1V. The input common-mode range of the device supports this value. And in your case, the VREF will also be 1.0V.

    Regards, Josh

  • One more question about that. Datasheet says that input common volate should be in range of 1V to 2V. Would't in my case when Vin- is 1V and Vin+ 0V, common voltage drop to 0.5V ? Can device still operat outside of specified range?

  • Yes, you are correct. I was still in 'differential mode' when I answered previous. Since you are driving it single-ended, the input common-mode range of the converter must be half that of the input signal amplitude range. Your signal range is 2Vpp, therefore the common-mode range must be 1V wide. Based on the input range of the ADC, this can be done, but only if Vin- is set to 1.5V.

    Regards, Josh