Other Parts Discussed in Thread: ADS1230, ADS1248
Please see attached schematic of the analogue I/Ps to the ADS1230. The operation of the circuit is as follows:
A constant current source provides current through R4 and a PRT connected at P2. The reference for the ADS1230 is developed across R4. The Analogue signal to be measured comes from the PRT. AINN is connected to Vss. The gain of the ADS1230 is 64. AINP and REFN are effectively at the same potential relative to 0v. According to the ADS1230 datasheet the reference voltage is purely determined by the voltage difference from REFP and REFN with no respect to 0v, is this correct?
This is circuit is not currently giving the correct output from the ADS1230, the output from the ADC is around 30 times smaller than expected. Is this something to with the configuration of the analogue section. If not, do you have any suggestions of what the problem may be? Note, for clarity I have only shown the analogue connections to the ADC.