I am using ADS5500 14-bit parallel configuration adc in my board interfaced to virtex-4 FPGA,The pin no 40 (DFS) of ADS5500 decides the output format whether straight binary or 2's complement .so in design it is set to 2's complement format now as per the datasheet of ADS5500 the output for 2's complemnt format should be in the range of 2000 to 1FFF and for straight binary it is 0000 to 3FFF.so in my case it should be around 1FFF for positive drive and 2000 for negative drive. but output of adc is coming around 3FFF.I've checked the DFS pin it is giving 1.24V which is set for 2's complement format .Please assist me Thanking you in advance