Hello,
I have an ADS1292RECG-FE PDK.
I want to make sure that the following deguggers are compatible:
1. ez430 (came as part of the Chronos Development Tool) - has Spy bi wire (6 pins)
2. ez430 (came as part of the ez430-F2013 Development Tool) - has 4 pins.
What are the differences between the their connectors? Is the ADS1292RECG-FE (which also have 6 pins can connect via the 4 pins connector)?