Hello,
I have a low power, high-speed application in which I need to sample at 250 MHz and want to conserve power by shutting off the voltage to my ADC until there is a signal of interest. I'm wondering, with the ADS5444-SP and the ADS5463-SP, how long after the proper voltages are applied for supply power that the ADC samples will be correct? If your answer includes the pipeline delay for the devices, please indicate this is the case. If these parts have a start up time beyond 100 nS, are there any other space qualified parts capable of 250 MHz sample rates that have faster start up times?