Page 19 of the data sheet has a somewhat vague mention of how to obtain single-ended unipolar output from the DAC, assuming it's still operating in I-V configuration. I would like to use this, so can someone explain what the final sentence "Node IOUT1 should be selected if a single-ended unipolar output is desirable." The earlier part of the paragraph explains that the op-amp will keep IOUT1 at virtual ground, so I don't understand how the circuit can continue to operate as an I-V converter. Perhaps I misunderstand what it means to "select" node IOUT1. Perhaps this is a typo?
My analog supply is 5V, and I would like the I-V output for full scale from the DAC to be 0V to 5V - i.e. single-ended unipolar. Is this possible with a single op-amp configuration attached to one or both of the IOUT pins of the THS5671?