What is the noise of the ADS1224? It says in the datasheet on page 3 that the noise is 0.8e-6 of the FSR. If I figure the FSR is a 5V span, this is 6uV-rms of noise, which would be 21 counts of noise or just over 4 bits of noise. I figure these calculations must be wrong because if there was 4 bits of noise there would be little reason to use this ADC over a 16-bit ADC with very low noise (I suppose decimation would give you a bit but not much) .