hello
it's very simple question but I'm a little confused
the Analog input pin is fixed ac-coupling??
I think it depend on external circuit using transformer-coupling or opamp such as THS4508
thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Siwon,
The input of the ADS41B29 is not 'fixed'. You are right, it depends on the driving circuit you use.
The EVM for instance uses a double-transformer input circuit which is by default optimised for high-bandwidth applications.
As explained in the EVM user guide (http://www.ti.com/lit/ug/slwu067c/slwu067c.pdf), you can also use an amplifier (for example THS45xx family) to drive the input. And, by removing the transformers and adjusting the driving circuit you can have a DC-coupled ADC.
Hope it helps,
Quentin