Hi all.
Although it is "Operating free-air temperature range and TA -40 85 degC" which have been indicated on the document (slas946.pdf) of "ADS5401",
Since it is written as "Operating junction temperature range TJ 150 degC", does the ambient air temperature operate,
if junction temperature is less than 150 degC at 100 degC?
For example, does the device operate in the state where junction temperature is 125 degC,
at the time of the ambient air temperature of 90 degC?
Is the value of tSU at that time changeful?
Best regards,
Hisa Kobayashi.