Hi there,
I have a question regarding the Voltage I can put on the part. P5 in the datasheet is confusing. The recommended voltages are 2.7V and 5.5V with Vss = 0, and for dual supply operation, +/-2.25V to +/-2.75V. The Max ratings show with Vdd to GND a 7V max, and with Vss to GND a -7V max.
It does not show recommended single supply if I use a negative voltage - like -5V, which is what I would like to use and not sure if this is possible. if it is not and I use +/- 2.5V, then is the I2C communication o.k. if I use 3.3V I2C? Is there a converter in the part if ave Bassettusing -5V only (if possible) so I can still communicate at 3.3V over I2C?
Thanks for the help
Dave Bassett