Hi all,
I am currently writing the firmware for the ADC08DL500. As I intend to use the device in extended control mode. From the datasheet I could see that the write-only register values are maintained while the device is in power down mode.
In order to save power I will actively use the power down mode of the device (I and Q channel will be down).
Now I am wondering whether it is possible to use the serial interface (i. e. write to the registers) during the power down mode.
Any suggestions would be greatly appreciated!
Thanks and best regards,
Gerald