Hi there,
I am trying to use a ADS 1225 to convert a differential signal with a sample time of 15ms. The data sheet of this adc says that in "high speed mode" the conversion time would be between 8ms and 13.3ms. In my current application I am having a bit more than 17ms. So we are far below the minimum required rate of 75SPS.
In a first attempt I thought that something else must be out of spec, if the adc doesn't manage the correct conversion time. So I tied the inputs at reference voltage 1.2V. The buffer is currently off and AVDD / DVDD are both at 3V. I have tried to just strobe the start pin or leave it high for continuous conversion, but this makes no difference. My question is now: What else could cause the ADS1225 to run out of spec?
Thanks for helping and best regards,
Tobias
P.S.: I will try to provide a small schematic to help for clarification.