This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ryuji,
Sorry for the delayed response; it appears we missed this post.
1) The logic level VOH is in reference to the VBD supply. This is a typographical error in the datasheet.
2) The GPIOs default to digital inputs when the device is powered up. A recommendation is to connect the unused GPIO's to GND via a pull-down resistor (~10kOhm)
I will verify/confirm with the design group regarding question (3), since the absolute maximum ratings are dependent on the internal ESD protection of the device. I will get back with a response ASAP.
Best Regards,
Luis
Hello Ryuji,
Regarding the absolute maximum ratings table, the spec for the Digital output to BDGND should be with respect to the digital supply
Best Regards,
Luis