Hi,
We have obtained questions of ADS7263 from our customers.
Could you please tell us as follows as soon as possible?
Q1. the Method to Connect to Device Controller
Could you please tell us the recommended method to connect to device controller by using SDOA and SDOB?
We consider to use TI products as the controller device.
For example, if we use TMS320C28346, how should we connect to this device by using SDOA and SDOB?
Please explain to us with reference to schematic diagram.
Q2. Input Voltage Range and External Pin Settings
We would like to use 5V as input voltage range in the pseudo-differential input mode.
Are the conditions(table 13. Output Data Format) described in the 28 pages of data sheet pseudo-differential input mode?
Moreover, we found that the description of "CHxxN = VREF = 2.5V".
In this case, should we connect CHxxN to REFIO1(or REFIO2)? or should we connect CHxxN to external voltage reference?
If we don't connet CHxxN to REFIO1(external voltage reference), is input voltage range 0V to +VREF?
Q3. the Performance Half-Clock Mode and Full-Clock Mode
When the full-clock mode is compared with the half-clock mode, is there any difference in performance?
We know that there is a difference with respect to INL and DNL for ADS8363.
How do you think about ADS7263(for example : INL, DNL, SINAD, SNR, THD, SFDR, etc.)?
Q4. Power on/off Sequence
The ADS7263 has two separate supplies(DVDD and AVDD).
Could you please tell us the recommended power-on and power-off sequence?
For example, should we supply the voltage to DVDD and AVDD at the same time?
Best Regards,
Kato