Hi,I have TSW1265EVM and TSW30SH84EVM.I want use TSW30SH84EVM clk6p output as TSW1265EVM clkin input.If the divider is 12,then clk6p is 2949.12/12=245.76MHz.
My questions is
1. Which CLK0 type should i use?LVPECL or LVCMOS? I think it maybe LVCOMS.There are nine types about LVCOMS,which one should i select?
2. How to set the TSW1265EVM registers?When I use configer file "250MHz_onboard_clock.txt" ,I get the result and finish my test. I want use external clock to test again now. Please help me.I hope you can send me a configer file which i can use.