Other Parts Discussed in Thread: THS5651A, SN74ALVC08, CDCE62005, DS92CK16, SN65LVDS104
I have create a layout for code testing base on THS5651A connected to a CPLD to 100 MHz clock. But I am getting wrong output.
The connections very simple:
10 digital lines with serial resistor 33 ohn.
clock 100Mhz also with a serial resistor to 33 ohn
"Sleep", "MODE" to digital ground
Digital supply a capacitor o.1 uF to digital ground
COMP2 to a capacitor 0.1uF to analog ground
Analog supply to capacitor to COMP1
Analog supply to a 2 capacitor (0.1uf and 7.7 uF) to analog ground,
Analog supply to a ferrite to analog power supply
pot 5k to a bias and ground
extio to a 2 capacitor (0.01uF and 0.1 uF) to a analog ground
extlo to analog ground
the two output with jumper to select a connection to 50 ohn precision resistor.
The test:
The CPLD and digital same supply to 3.15 V, the analog supply to 5 V.
The clock is taken to the THS at 100 MHz, at about 880 mVpp
The 10 digital lines at about 3.2 Vpp at 2500 ns = 2.5us
The Analog supply is taking about 5mA
Now the result is about 3 set of frequency, i can see the clock at the output at about 100mVpp with lot of distortion
there is a set of signals at about 1.4 us signal that I cannot trigger
and there is at 2ms and 100mVpp signal very distort also.
Should I be seeing a signal at around 10 usec? also there is lot of noise and distortion, What am I missing? Thanks